Search FAQs
Can I buy the 2510KW2H's enclosure only?
Issue:
Is an enclosure for 2510 KW2H sold separately?
Product Line:
2510 type K manual switches
Environment:
Products sold and used in the United States
Cause:
Enclosure needed for the 2510 type KW2H manual switch
Resolution:
Enclosure Complete (see notes) series B 31057-529-56 The Series A, Class 2510 Type KW2H, NEMA 4, watertight device, was obsoleted 1-14-2002 and was replaced with a Class 2510 KW2H Series B.
Series B consists of a redesigned enclosure (box) and cover assembly. The new Series B is identical to the Series A except for the overall width of the enclosure (box) is slightly wider - wider by only .15`` (5/32``). The Series B cover will not mount to the Series A box. The mounting holes for the Series B device are identical to the old Series A device.
Important Note:
Series A covers and boxes are NOT interchangeable with Series B devices due to the redesign. This is due to changes in location of the four (4) cover mounting screws.
Repair Parts:
Description: Part Number:
Replacement Toggle Kit 9998 HW1
Enclosure Complete (see notes) 31057-529-56
Cover Gasket Only 31101-155-01
Toggle Type Starter (3 Pole) 2510 KO2
Notes:
The enclosure complete will be the Series B design. The mounting holes will be identical to the old Series A.
The Series B cover will not fit onto the old Series A box, which will require replacement of the old box.
The only Series A cover available is one which has a pilot light lens. This could be used as a replacement if the
customer does not want to replace the box which probably has hard conduit connected to it.
Part number for the pilot light cover only is 31057-529-53.
Is an enclosure for 2510 KW2H sold separately?
Product Line:
2510 type K manual switches
Environment:
Products sold and used in the United States
Cause:
Enclosure needed for the 2510 type KW2H manual switch
Resolution:
Enclosure Complete (see notes) series B 31057-529-56 The Series A, Class 2510 Type KW2H, NEMA 4, watertight device, was obsoleted 1-14-2002 and was replaced with a Class 2510 KW2H Series B.
Series B consists of a redesigned enclosure (box) and cover assembly. The new Series B is identical to the Series A except for the overall width of the enclosure (box) is slightly wider - wider by only .15`` (5/32``). The Series B cover will not mount to the Series A box. The mounting holes for the Series B device are identical to the old Series A device.
Important Note:
Series A covers and boxes are NOT interchangeable with Series B devices due to the redesign. This is due to changes in location of the four (4) cover mounting screws.
Repair Parts:
Description: Part Number:
Replacement Toggle Kit 9998 HW1
Enclosure Complete (see notes) 31057-529-56
Cover Gasket Only 31101-155-01
Toggle Type Starter (3 Pole) 2510 KO2
Notes:
The enclosure complete will be the Series B design. The mounting holes will be identical to the old Series A.
The Series B cover will not fit onto the old Series A box, which will require replacement of the old box.
The only Series A cover available is one which has a pilot light lens. This could be used as a replacement if the
customer does not want to replace the box which probably has hard conduit connected to it.
Part number for the pilot light cover only is 31057-529-53.
Released for:Schneider Electric Canada
Explore more
Product:
Explore more
Product: