{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the single-phase and three-phase SDSA surge arrestors be used on a 50 Hz system?
Issue:
Verification if the single-phase and three-phase SDSA surge arrestors are rated for use on a 50 Hz system.

Product Line:
Surge Protective Devices (SPDs)

Environment:
Maintenance

Resolution:
Indeed, the SDSA surge protectors are suitable for use on systems operating at 50 or 60 Hertz.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: