{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the difference between the EIK1 and EIK2 Electrical Interlock Kit?

Article available in these languages: Spanish

Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Environment:
Electrical Interlock Accessory

Cause:
Application

Resolution:
Electrical Interlock kits with "-1" suffix has one normally open (1 NO) and one normally closed (1 NC) contacts. Kits with "-2" suffix has 2 normally open (2 NO) and 2 normally closed (2 NC) contacts.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.