{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement interior deadfront trim for a QON442MS400 load center interior?<br />
Issue:
Design repair parts

Product Line:
QO load centers

Resolution:
The interior deadfront trim will consist of two separate parts. Use 8011632478 for the Main Breaker deadfront trim. Use NQODRPL42L4 for the Branch Breaker deadfront trim. For deadfront trim mounting screws use 8002506701 (6 required, but are included with the trim part numbers).

Schneider Electric Canada