{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the difference between AFI and GFI circuit breakers?

Issue:
Product Design Features
Product Line:
Miniature Circuit Breakers
Resolution:
The AFI is a UL listed circuit breaker designed to mitigate the effects of arcing faults. It is required by UL to protect against arcs between current carrying conductors above 75 A (Square D AFI protects from arcs above 50 A), and may trip on leakage to ground with a minimum threshold of 30 to 50 mA.
The GFI is a circuit breaker UL listed for interrupting the circuit when more than 6 mA of ground fault leakage is detected.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: