{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the rating of the number of switching operations (endurance operations or horsepower-overload operations) for Square D, 30-60 A, Heavy Duty, F-Series Safety Switches?
Issue:
Application

Product Line:
HD Safety Switch

Cause:
Application

Resolution:
For safety switches, the standard for design and testing of the number of switching operations is governed by UL98 and NEMA KS-1.There are two separate tests: (1) Endurance Test and (2) Horsepower-overload test. The below table shows the minimum number of operations required (OFF to ON to OFF) by UL and NEMA. For the endurance test, however, Square D 30 and 60 A F-Series Safety Switches exceed the UL and NEMA requirements by more than 3 times the total (see below table):

NUMBER OF OPERATIONS
Square D Safety Switches (F-series)
30A-60A, Heavy Duty

Endurance Test # of OpsHP Test # of Ops
Test StandardAt Rated Load*No LoadTotal (L + NL)At Rated HP**
UL600040001000050
NEMA800070001500050
Square D8000420005000050







* endurance test done at switch rated load current
** horsepower test - make/break motor inrush/locked rotor current at rated HP
For 100A series F Heavy Duty safety switches, see FA99790
For 200A series F Heavy Duty safety switches, see FA99791
For 400A series E Heavy Duty safety switches, see FA99792
For 600A series E Heavy Duty safety switches, see FA99819
For 800A series E Heavy Duty safety switches, see FA99821
For 1200A series E Heavy Duty safety switches, see FA99822

Schneider Electric Canada