{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the HOM2150 and HOM2200 breakers be used as a branch circuit breaker in a Homeline load center or CSED?

Article available in these languages: Spanish

Issue:
Product Design Features

Product line:
Homeline branch breakers

Environment:
Branch breakers

Cause:
Application

Resolution:
CSED = Combination Service Entrance Devices
MB = Main Breakers


No, the HOM2150 and HOM2200 CANNOT be used as branch circuit breakers. These breakers are designed as Main Breakers that were used in obsolete design HOMELINE load centers. But they are still used in a few CSED catalog numbers as the main breakers.

NOTE: The high amperage Homeline branch breakers are part numbers HOM2150BB, HOM2175BB and HOM2200BB and these breakers can ONLY be used in the Homeline CSED that are designed to accept them, see current digest and/or wiring diagram of each specific catalog number for use.

Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: