{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the number of switching operations of Square D, 800A, heavy duty, E-Series safety switches?
Issue:
Product design features

Product Line:
Heavy Duty Safety Switches

Resolution:
For safety switches, the standard for design and testing of the number of switching operations is governed by UL98 and NEMA KS-1.There are two separate tests: (1) Endurance Test, and (2) Horsepower-overload test. The below table shows the minimum number of operations required (OFF to ON to OFF) by UL and NEMA, as well as the number of operations required by Square D.

NUMBER OF OPERATIONS
Square D Safety Switches (E-series)
800A, Heavy Duty
Endurance Number of OperationsHP Number of Operations
Test StandardsUnder Load*No LoadTotal (Loaded + Unloaded)At Rated HP**
UL5003000350010
NEMA6002900350010
Square D6003000360010

* endurance test done at switch rated Load current
** horsepower test - make/break motor inrush/locked rotor current at rated HP

Schneider Electric Canada