{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the response time of the Multi-9 undervoltage relay?
Issue:
Tripping time of the Multi-9 UVR

Product Line:
Miniature Circuit Breakers

Resolution:
The auxiliary trip units will trip in a response time less than 10 ms if the input voltage decreases between 70% and 35% of Un for more than 3 ms.

Schneider Electric Canada