Search FAQs
Will the BMENOR2200H swap Ip in M580 Hot Standby?
Issue
When the BMENOR2200H is used in a Hot Standby configuration does the Ip address stay or automatically swap with an M580 switchover?
Product Line
Modicon M580, Modicon X80
Resolution
The Ip address of the standby module is the primary NOR address +1 and this will automatically swap from primary to standby. Must use CE15.1, 15.0SP1 or Hot Fix V150_HF_BMENOR2200H must be installed with Control Expert V15.0 and at least firmware version 1.70 loaded into the module.
Released for:Schneider Electric Canada
Explore more
Product:
Range:
Explore more
Product:
Range: