Can solar be added on the bottom section of the interior of the Energy Center?
Solar can be added to the bottom section up to 120 A per the 120% rule. Installer will need to check with AHJ and the homeowner’s utility for the maximum interconnection agreement.
Released for:Schneider Electric Canada
Explore more
Product:
QOWC60M200PFY
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.