{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the purpose of the top and bottom sections of the Energy Center?
Issue:
Why are there two sections in the Energy Center and what are their purposes?

Product Line:
Energy Center

Resolution:
The purpose of the top and bottom section is to provide a backup ready section and a non-backup ready section that can easily be interchangeable from partial home and whole home backup.

In addition, the submain disconnect allows for increased solar backfeed of 120 A per section, with a total of 240 A for the entire panel without having to do a line side splice or panel upgrade.

Schneider Electric Canada