undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What generators are compatible with the Energy Center?
Any portable generator up to 50 A can be connected to the Energy Center via a manual interlock kit (QO2DTEC) and a suitable inlet port. Standby generator support is provided by the battery backup interface and generators up to 22 kW are supported, which require closed contact run command.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: