The Rocker Dimmer is designed to connect with a standard mechanical single-pole switch where only the neutral and traveler wires are connected. This significantly reduces the cost of supporting a 3-way application. Installation Bulletin
Do X Series Wiring Devices support copper-clad aluminum (CCA)?