The switch module body is white, inside there is a light almond actuator. Simply press the actuator at the top or bottom to turn on or off the load. If the actuator requires you to hold it in the on position, then you have a momentary switch.
Do X Series Wiring Devices support copper-clad aluminum (CCA)?