{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a limit to the number of X Series Wi-Fi devices that can be installed on a home network?

The largest real-world limitation on the number of devices is the quality of the home Wi-Fi network. Typically, 20 Wi-Fi devices can be expected. Please refer to the Connected Home offer for more details.

Do X Series Wiring Devices support copper-clad aluminum (CCA)?

Schneider Electric Canada

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: