{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I use my X Series connected devices Wi-Fi Switch or Dimmer on a 3-way circuit?

Both the Wi-Fi Switch and Dimmer are designed to connect with a standard mechanical single-pole switch where only the neutral and traveler wires are connected. This significantly reduces the cost of supporting a 3-way application. Please refer to the Connected Home offer for more details.

Do X Series Wiring Devices support copper-clad aluminum (CCA)?

Schneider Electric Canada

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: