{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to troubleshoot a loss of communication on the Wiser Energy Monitor?
Issue:
How can troubleshooting be done on a loss of communication on a Wiser Energy Monitor?

Product Line:
Wiser

Resolution:
If you hear repeated beeps or no sound at all, this may mean that Wiser energy monitor was not properly installed. Please turn off the breaker that the Wiser energy monitor is connected to and check the following:

The red and black power wires are connected to a 240 Vac breaker
The white wire is connected to the neutral bus
All cables are connected to the Wiser energy monitor
The Wiser energy monitor breaker and solar breakers are both ON
The labels on the current sensors are facing the same direction (either both towards or both away from the breakers). If your service mains have loops, please follow the wires to determine the appropriate direction.

If all of the above is correct and the Wiser energy monitor still does not chime or beep, reset the breaker that it is installed on and have your installer check for a flashing LED near the monitor's antenna port. This flashing LED indicates that the monitor is in "pairing mode" and is ready to connect to your mobile device via Bluetooth. You are now ready to set up Wiser Energy.

The Wiser energy monitor will only beep or chime during the installation and registration process. Once the monitor has been registered to an account, it will no longer beep or chime when powering up.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: