{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the stainless steel type for the Square D EMA and ASCO 460 Surge SPD enclosure?

The EMA Series Stainless Steel is 304 SS not 316 SS 

What’s the difference between 304 and 316 stainless steel?

The simple answer is 304 contains 18% chromium and 8% nickel while 316 contains 16% chromium, 10% nickel and 2% molybdenum. The molybdenum is added to help resist corrosion to chlorides (like sea water and de-icing salts)   https://www.nemaenclosures.com/blog/304-and-316-stainless-steel/

https://www.polycase.com/techtalk/steel-enclosures/304-vs-316-stainless-steel.html

We do not have special builds for 316 stainless steel for the EMA and 460 SPDs.

 

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top