{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum voltage for NF panels?
Issue:
Can NF panels be used in a voltage system higher than 480Y/277V?

Product Line:
Panelboards

Resolution:
New NF panelboards can now be used on 600Y/347 Vac systems. The E frame circuit breakers now have the same rating, just use the breaker with the 6 as the voltage code (e.g. EDB36015).

Schneider Electric Canada