{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the minimum speed to actuate an XB5R Wireless pushbutton?
Issue:
If the button XB5R is pressed slowly, the receiver does not get the signal.

Product line:
Push Buttons and Operator Interface

Environment:
Harmony 22 mm XB5R/XB4R Wireless Push Buttons

Resolution:
The maximum force is 10N and the minimum actuation speed is 0,1m/s.

Actually, if the operator actuates very lowly the transmitter, it can affect the frames transmitted.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: