{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does Square D offer Line Side Barrier Kits for the QOM2 circuit breaker enclosures?

Issue:
Service entrance barrier kit for enclosed QOM2 breaker

Product Line:
QOM2 enclosures

Resolution:
Line Side Barrier Kits are NOT available for the QOM2 Circuit breaker enclosures. Consider using enclosed PowerPacT Q-frame breakers instead, the catalog numbers Q2150MRBE or Q2200MRBE or Q2200RBE or Others.

NOTE: The carton Label for the QOM2 Enclosures, that is located on the outside of the carton for the devices states "Non-Service Entrance Device", So customers should see and read this label before obtaining the device for use in Service Entrance Applications. See below a visual of the carton label wording.
Carton Label visual

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: