{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
SDSA1175 SDSA1175T Selection, Voltage, Wiring, and Ground

Problem: Choosing between SDSA1175 or SDSA1175T for ordering.


Product Options: SDSA1175 120/240V or SDSA1175T 120V surge protection devices (SPDs) with a surge current rating of 36kA per phase.


Environment: 120V 1P Single Phase or 240/120V 1P Split Phase.


Reason: Ordering the wrong SPD requires return/exchange, if possible. One SPD cannot substitute for the other. It is crucial to order the correct SPD with the appropriate voltage code.

  • It is essential to order the appropriate SPD with the correct voltage code.  If you have 120V 1P, the SDSA1175T is the correct SPD, not the SDSA1175 120/240V.
  • It is essential to order the appropriate SPD with the correct voltage code.  If you have 240/120V 1P, the SDSA1175 is the correct SPD, not the SDSA1175T 120V.


Solution: SDSA1175 and SDSA1175T units lack a green wire for connection to the electrical system ground. The neutral wire, usually a larger #AWG wire, provides a lower impedance path back to the N-G Bond. SDSA1175 and SDSA1175T have a white neutral wire, used for surge current dissipation back to the electrical system service entrance.


Details:

  • SDSA1175: Three-wire surge suppressor for 120/240 VAC services (2 phase conductors, a neutral, and no ground).
  • SDSA1175T: Two-wire surge suppressor for 120 VAC services (1 phase conductor, a neutral, and no ground).


Product Family   -   SDSA1175 SDSA1175T

The SDSA1175 is designed for 120/240V single phase (L1-L2 & N) 36kA

Schneider Electric Canada

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: