Search FAQs
Can Control Expert connect to multiple PLCs via USB?
Issue
Is it allowed to connect to multiple instances of Control Expert to multiple PLCs using USB connections?
Product Line
Control Expert
Resolution
It is not allowed to connect more than one PLC over USB. See the warning below.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: