Search FAQs
How to Clear an M580 Hot Standby controller
Issue
Will be adding a Standby PLC to an existing Primary and would like to clear the program that is in the PLC which will be Standby.
Product line
Modicon M580
Resolution
There is a switch on the back of the controller that can be used to clear the program from the M580 Hot Standby controllers.
Released for:Schneider Electric Canada
Explore more
Product:
Explore more
Product: