{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
In the new style MPU Mini Power-zones, is it possible to change the primary 2-pole breaker to a 3-pole version?
Product Line:
Mini Power-zone

Environment:
Low Voltage Transformers

Cause:
Looking at MPU15S40F which has a 2-pole HDL breaker. The source voltage is a corner-grounded Delta which requires a 3-pole circuit breaker. Need to know if it can be swapped out with a 3-pole version.

Resolution:
The MPUs have not been UL tested and approved using a 3-pole main breaker in the single-phase units. So since they are UL listed as built with the HDL26060, we can not advise a customer to change the design on them. The hole pattern is also different on the 2-pole and the 3-pole HDLs, so the sheet metal back pan would have to be physically re-drilled to accommodate the larger breaker, which is an even further physical modification we can not endorse. The UL rules and regulations are our guiding principle regarding modifications to Transformers in almost every situation.

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: