{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why is BMXNRP0200 not included in documentation printout?

Issue

With Control Expert, when Printing out an M580/M340 configuration that includes BMXNRP020x modules, they do not show in the configuration.

Product Line

Control Expert, Unity Pro

Resolution

Since the BMXNRP020x modules are not really part of the configuration they are not included. They do not actually interact with the M580/M340 at all across the backplane. They simply take CPS power from the backplane to power up. You could take the NRP out of the PAC backplane and put in on its own backplane with simply a PS and it would still work the same way. You are not required to map it even if it resides in one of the CPU or CRA backplanes as it does not interact. It is strictly mapped so that you know it is there, no functional reason.

Schneider Electric Canada

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: