Product Line:
EX/EXN Transformer
Environment:
Low Voltage Transformer
Cause:
Replacement for the top, rear and front panels for EXN75T3HCU enclosure.
Resolution:
Transformer Dry Enclosure Part 20M Base = PHA35455
Transformer Dry Enclosure Part 20M Front = PHA35456
Transformer Dry Enclosure Part 20M Rear = PHA35457
Transformer Dry Enclosure Part 20M Top = PHA81739
Transformer Dry Enclosure Part 20M Side = PHA35458
Note: To order the replacement front with the proper nameplate for the transformer, make sure to provide the following information Serial Number and Date code. A picture of the nameplate placed on the front panel and pictures of the coils labels is required to be included with the purchase order.