{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Using Control Expert how can two INT variables become a DINT?

Issue

I have two INTs which would represent the LOW and HIGH word of a Double Integer, how can I combine them into a Single DINT variable?

Product Line

Control Expert

Resolution

The function INT_AS_DINT can be used to accomplish this task.

Schneider Electric Canada