To better support modernization with a high input voltage threshold from legacy Quantum 100~120V AC discrete input modules, we released the BMXDAI16142. It is fine-tuned from BXMDAI1614 to focus on input voltage range 100 to 120 V AC 60Hz. The BMXDAI16142 follows most characteristics of the BMXDAI1614. It’s delivered in the same X80 new high form factor as the BMXDAI1614 and is supported on M340, M580 and Quantum EIO X80 drops.
In the programming software it is mapped as a BMXDAI1614.
It provides below features and benefits to customers:
· High density AC isolated inputs reduce overhead cost of backplanes, panel space and cabinets etc.
· Advanced diagnostics with open wire detection and supply monitoring
· Easy legacy Quantum modernization with compatible channel counts, isolation, wiring and voltage rating
· Robustness with channel isolation and in hardened version