{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Recommendations and Clarifications for SPD Circuit Breakers and Wire Sizing.

Circuit Breaker and Wire Sizes for Surge Protection Devices

Schneider Electric Square D Surgelogic and ASCO 400 series surge protective devices (SPDs) incorporate individually fused and thermally protected metal oxide varistors (MOVs). This feature provides superior withstand capability for systems with unstable power, without compromising transient clamping performance. The component level fusing also allows the surge protector to be directly connected to the electrical bus without external overcurrent protection. When connecting via a breaker, which acts as a service disconnect, consult local electrical codes to select the appropriate size based upon the wire gauge to be used. Based upon National Electric Code (NEC), factory recommendations are listed above. For technical support contact SPDTAG@se.com (800) 577-7353.

Schneider Electric Canada