Issue:
Tesys Island EIP bus coupler LED's meaning
Product Line:
Motor Management system Tesys Island
Environment:
IEC Contactors and Starters
Resolution:
TPRBCEIP EtherNet/IP™ Bus Coupler LEDs
LED | Color | State | Description |
---|---|---|---|
PWR | Dual LED, Yellow/Green | ||
Yellow | Static | The system is booting. | |
Green | On | Operating system running. | |
Off | Off | The power supply for the device is missing, or the hardware is not operational. | |
Yellow | Static (5 s) | Identification of the connected bus coupler following a Locate command. Other LED behavior is overridden for 5 s. | |
Yellow | Flashing | The system is in Force Mode. | |
MS Name in the device drawing: COM 0 | Dual LED, Red/Green | ||
Green | On | Device operational: The device is operating correctly. | |
Green | Flashing | Standby: The device has not been configured. | |
Red | On | Major event: The device has detected a non-recoverable major event. | |
Red | Flashing | Minor event: The device has detected a recoverable minor event. NOTE: An incorrect or inconsistent configuration is a minor event. | |
Red/Green | Flashing | Self-test: The device is performing its power-up testing. | |
Off | Off | No power: No power is supplied to the device. | |
NS Name in the device drawing: COM 1 | Dual LED, Red/Green | ||
Green | On | Connected: The device has at least one established connection (even to the message router). | |
Green | Flashing | No connections: The device has no established connections but has obtained an IP address. | |
Red | On | Duplicate IP: The device has detected that its IP address is already in use. | |
Red | Flashing | Connection timeout: One or more of the connections targeting this device have timed out. This condition is cleared only if all timed-out connections are reestablished or if the device is reset. | |
Red/Green | Flashing | Self-test: The device is performing its power-up testing. | |
Off | Off | Not powered, no IP address: The device does not have an IP address, or is powered off. | |
LINK/RJ45 ETH and TER Ports | LED, Green | ||
Green | On | The device is connected to the Ethernet network. | |
Off | Off | The device is not connected to the Ethernet network. | |
ACT/RJ45 ETH and TER Ports | LED, Yellow | ||
Yellow | Flashing | The device is sending or receiving Ethernet frames. | |
BS/ERR | Black | Off | No connection to the internal bus. |
Blinking green | On with COM | Connection/communication to the internal bus. | |
Steady green | On | Connection to the internal bus. |
TPRBCPFN PROFINET® Bus Coupler LEDs
LED | Color | State | Description |
---|---|---|---|
PWR | Dual LED, Yellow/Green | ||
Yellow | Static | The system is booting. | |
Green | On | The operating system is running. | |
Green | Flashing (3 s) | The bus coupler received a DCP signal command from the PROFINET network. | |
Off | Off | The power supply for the device is missing, or the hardware is not operational. | |
Yellow | Static (5 s) | Identification of the connected bus coupler following a Locate command. Other LED behavior is overridden for 5 s. | |
Yellow | Flashing | The system is in Force mode. | |
SF Name in the device drawing: COM 0 | Dual LED, Red/Green | ||
Red | On | The system transitions to the status, Major Event State Active (problem indicator within a Diagnosis alarm). | |
Red | Flashing (3 s) | The DCP service is being initiated. | |
Off | Off | No system errors and no ongoing DCP configuration. | |
BF Name in the device drawing: COM 1 | Dual LED, Red/Green | ||
Red | On | No configuration; low-speed physical link; or no physical link. | |
Red | Flashing | No data exchange. | |
Off | Off | — | |
LINK/RJ45 PFN and TER Ports | LED, Green | ||
Green | On | The device is connected to the Ethernet network. | |
Off | Off | The device is not connected to the Ethernet network. | |
ACT/RJ45 PFN and TER Ports | LED, Yellow | ||
Yellow | Flashing | The device is sending or receiving Ethernet frames. | |
BS/ERR | Black | Off | No connection to the internal bus. |
Blinking green | On with COM | Connection/communication to the internal bus. | |
Steady green | On | Connection to the internal bus. |
TPRBCPFB PROFIBUS® Bus Coupler LEDs
LED | Color | State | Description |
---|---|---|---|
PWR | Dual LED, Yellow/Green | ||
Yellow | Static | The system is booting. | |
Green | On | The operating system is running. | |
Off | Off | The power supply for the device is missing, or the hardware is not operational. | |
Yellow | Static (5 s) | Identification of the connected bus coupler following a Locate command. Other LED behavior is overridden for 5 s. | |
Yellow | Flashing | The system is in Force mode. | |
MS Name in the device drawing: COM 0 | Dual LED, Red/Green | ||
Green | On | Device operational: The device is operating correctly. | |
Green | Flashing | Standby: The device has not been configured. | |
Red | On | Major event: The device has detected a non-recoverable major event. | |
Red | Flashing | Minor event: The device has detected a recoverable minor event. NOTE: An incorrect or inconsistent configuration is a minor event. | |
Red/Green | Flashing | Self-test: The device is performing its power-up testing. | |
Off | Off | No power: No power is supplied to the device. | |
COM Name in the device drawing: COM 1 | Dual LED, Red/Green | ||
Green | On | Cyclic communication. | |
Red | Flashing (cyclic) | No communication—connection error. | |
Red | Flashing (acrylic) | Not configured. | |
Off | Off | — | |
LINK/RJ45 TER Port | LED, Green | ||
Green | On | The device is connected to the Ethernet network. | |
Off | Off | The device is not connected to the Ethernet network. | |
ACT/RJ45 TER Port | LED, Yellow | ||
Yellow | Flashing | The device is sending or receiving Ethernet frames. | |
BS/ERR | Black | Off | No connection to the internal bus. |
Blinking green | On with COM | Connection/communication to the internal bus. | |
Steady green | On | Connection to the internal bus. |
This information can be found on the TeSys Active TeSys island – Digital Motor Management Solution – System, Installation, and Operation Guide.
Released for:Schneider Electric Canada