Issue:
Can the SIL starters be used as standard starters?
Product Line:
Motor Management system Tesys Island
Environment:
IEC Contactors and Starters
Resolution:
No, the SIL interface module is required for the proper operation of a SIL Starter.
If no SIL interface is desired, use a standard TPRST*** starter.
Can the SIL starters be used as standard starters?
Product Line:
Motor Management system Tesys Island
Environment:
IEC Contactors and Starters
Resolution:
No, the SIL interface module is required for the proper operation of a SIL Starter.
If no SIL interface is desired, use a standard TPRST*** starter.