Issue:
I cannot add an avatar to the configuration of my Island in Somove
This message shows up:


Product line:
IEC Contactors and Starters
Environment:
Tesys Island Motor management solution
Solution:
As the messages state, there is something about your configuration which means it is too large/invalid. As a reminder, the constraints are:
Suggest to remove an avatar, remove an IO module, or split up into two islands if this constraint arrives
I cannot add an avatar to the configuration of my Island in Somove
This message shows up:
Product line:
IEC Contactors and Starters
Environment:
Tesys Island Motor management solution
Solution:
As the messages state, there is something about your configuration which means it is too large/invalid. As a reminder, the constraints are:
- Maximum of 21 bus devices, (20 starters + 1 VIM or 20 starters + 1 SIM). 21 starters is invalid
- Maximum of 5 Frame 3 devices active (a reverser avatar counts as 1 frame 3, because only one is ever on at a given moment)
Suggest to remove an avatar, remove an IO module, or split up into two islands if this constraint arrives
Released for:Schneider Electric Canada