{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for a Q2200MRBE series E05 enclosure?
Issue:
Repair parts

Product Line:
Single phase service entrance enclosures

Resolution:
Only the parts listed below are considered field replaceable.
Closing cap for top endwall - 4023000201
Closing cap mounting screws - 2142720241 (2 are required)
Deadfront trim -  4050578201 (no labels are attached)
Deadfront trim mounting screw - 4020513001k (pack of 10, only 1 is required)
Service disconnect label - 4026858006
Neutral assembly - 4051520151
Neutral assembly mounting screws - 2190320160 (2 are required)
200 A Circuit breaker - QDL22200
Circuit breaker mounting screws - 4812112150A (includes both 2" and 3" screw)
PKSB1Q2 - (1) Service entrance barrier & (1) emergency disconnect label

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: