Search FAQs
Altivar and Altistart keypad connection in Modbus Serial port
Issue:
Does the VW3A1111 keypad can be connected in the Modbus serial port?Product line:
Altivar Process, ATV630, ATV930, ATS480
Environment:
All models
Cause:
Costumer would like to know if it's possible to connect the keypad in the Modbus Serial port instead of connecting it on the front of the drive.
Resolution:
Yes, you can connect the keypad in the Modbus port, you only need to confirm the baud rate, the word order and the modbus format.
Baud rate: 19200bps
Terminal Modbus word order: Modbus Word Order ON
Modbus format: 8 bits even parity 1 stop bit
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: