Issue:
RMCV60BD instruction sheet does not show the wiring instructions.
Product line:
Interface and Control Relays
Environment:
Harmony Analog SE relays
Resolution:
RMCV60BD instruction sheet does not show the wiring instructions.
Product line:
Interface and Control Relays
Environment:
Harmony Analog SE relays
Resolution:
See the attached wiring schematic and description:
> A1(+) & A2(-) are the control voltage terminals for 24 V DC (+/- 20 %).
> The switch at the top is selected based on the input voltage type, that is AC or DC.
> The input voltage coming from your battery is wired to only one of the V# terminals depending on the voltage range. Wire (+) to terminal:
- V1 if input voltage is between 0...50 V
- V2 if input voltage is between 0...300 V
- V3 if input voltage is between 0...500 V
and (-) to terminal IPG.
> The switch a the bottom is selected based on the output type
> The output terminals are Vo (+) and OPG (-)