{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there an option to safely engage and disengage power stabs from the vertical bus with the bucket/unit door closed in a Motor Control Center?

Issue:
Option to safely engage and disengage power stabs from the vertical bus with the unit door closed for MCC

Product Line:
Motor Control Centers

Environment:
Maintenance

Cause:
Unit compatibility and ordering

Resolution:
Yes, only if the bucket is a Closed Door Racking (CDR) unit. This solution allows the user to disengage or engage the bucket with the door closed using a racking handle, an electric screwdriver and/or a remote racking device to perform this action from outside of the flash boundary.

CDR units are available for standards, arc-resistance, and intelligent MCCs, as with Starters sizes 1 – 4, AltistartTM 22 and 48, AltivarTM 61 and 71 and it is Compatible with Model 5 legacy MCCs. Contact your local distributor to get a CDR unit or call 888-SQUARED (888-778-2733) to retrofit an existing unit.

Consult following resources for more info: Closed Door Racking (CDR) Unit for Model 6 MCC Installation and User Guide & Closed Door Racking Brochure

Schneider Electric Canada