{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the CBGS-0 Gas Insulated Switchgear available for outdoor installation?

Issue:
Outdoor CBGS-0 Gas Insulated Switchgear availability

Product Line:
MV Switchgear

Environment:
CBGS-0 Gas Insulated Switchgear

Cause:
Is there an outdoor option for CBGS-0 Gas Insulated Switchgear?

Resolution:
No, the equipment is available in a variety of arrangements in enclosures designed and constructed for Type 1, indoor use. If this switchgear is intended to be installed outdoor, install this CBGS-0 switchgear in a Walk-in, Power Zone enclosure or have a third party build enclosure around it.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: