Issue:
LIM Error Code 9.1
Product Line:
Medical Products
Environment:
IGD
Cause:
Troubleshooting
Resolution:
Error code 9.1 "Line Ratio is Low" means either there is something wrong with the Line Voltage coming into the LIM unit or this LIM unit has reached its serviceable tolerance limit and needs to be replaced.
In this case, what you can do is taking the faceplate off the LIM and checking the DIP switch settings, you can see the information on this switch on Page 9 of IsoGuard Series D LIM Bulltetin - 43134-017-02 document.
If DIP settings are OK and the problem persists the existing IsoGard D LIM needs to be replaced. Reach out to your local distributor for our latest IG6 offer.