Is the ACSC fan system fault tolerant?
Issue:
Is the ACSC fan system fault tolerant?

Product line:
ACSC100, ACSC101

Environment:
InRow Cooling

Cause:

Resolution:
Yes, there are 2 power supplies in the unit for the condenser and evaporator fans. If 1 fails the other can supply 70% of the maximum power needed, so maximum fan capacity would be reduced approximately 30%. A user can replace the failed power supply from the front of the unit while the ACSC is still in operation. The evaporator fans are also hot swappable.

Schneider Electric Chile

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: