What is the maximum cable bundle diameter allowed by the the AR8621 Toolless Hook & Loop Cable Manager, and how long are they?
Issue:
This information is needed to determine what size cable bundles can attach to each AR8621.

Product Line:
NetShelter Cable Management

Environment:
AR8621

Cause:
The maximum cable bundle o.d. is not noted in the technical specs.

Resolution:

The 18" hook & loop cable ties included in the AR8621 support a maximum cable bundle of diameter of 6 inch.

Schneider Electric Chile

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: