Can the NetShelter AV busbar be installed into other NetShelter cabinets?
Issue:
AR8395 mounts to the accessory rail in the cabinet so it should be able to install into any NetShelter cabinet.

Product Line:
AR8395

Environment:
All versions and serial ranges.

Cause:
AR8395 description says that it's for the NetShelter AV cabinets.

Resolution:

The AR8395 can be installed into any NetShelter cabinet that has 20U vertical mounting space available.

Schneider Electric Chile

Explora más
Rango:
Artículos que pueden ser útiles
Explora más
Rango: