What is the replacement keyed operator for the XB3D cam switch?
Issue:
XB3D keyed operator broke

Product Line:
Push Buttons and Operator Interface

Environment:
Cam switches Harmony Pushbuttons

Resolution:
No replacement parts are available for the XB3D cam switches.  These were custom built as a complete device only.

NOTE the XB3D are obsolete with no direct replacement.  Consider the 9003K2 cam switch product line.  See attached file.

Schneider Electric Česká republika

Přílohy
9003CT1301R0616 Cam K2.pdf [1.43 MB]