undefined undefined
{}

Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
Jak vám dnes můžeme pomoci?
Is there a clear cover for a 22mm E-stop mushroom button?
Issue:
Cover for XB4 / XB5 emergency stop push button

Product Line:
22mm Push Button

Environment:
XB4/XB5 Harmony 22mm Push Buttons

Cause:
Application is calling for a clear plastic protector to cover operator.                          

Resolution:                                                                 
Covers are not available. We do not provide anything that will hinder access to an E-stop or Emergency operator.