{}

Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
Jak vám dnes můžeme pomoci?
Does the AR2144BLK or AR2145BLK NetShelter VX Seismic have leveling feet or castors available as an accessory?
Issue:
A customer may ask if castors are an accessory for our NetShelter VX cabinet.

Product Line:
NetShelter VX

Environment:
All versions and serial ranges.

Cause:
Castors can be used to move the cabinet much eaqsier.

Resolution :

The NetShelter VX cabinets do not offer castors as an accessory. These cabinets are approved for NEBS GR-63-CORE seismic installation, which does not include the use of castors.
Also see attached document.

Schneider Electric Česká republika

Přílohy
AR2144BLK AR2145BLK Feet and Castors.doc [102 KB]