{}

Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
Jak vám dnes můžeme pomoci?
What is the transfer time of the Back-UPS?
Issue:

What is the transfer time of the Back-UPS?

Product Line:

Back-UPS, Back-UPS PRO

Environment:

N/A

Cause Resolution:

Tranfer time refers to the duration in time it takes the UPS to switch from one state (i.e. Onbattery, Online...) to another.

The transfer time of the BK CS and ES units is 10-12 milliseconds.
The transfer time of the BK RS units is 6-8 milliseconds.