What is the part number for the cooling fan for the ATV61HD30N4?
Issue:
ATV61HD30N4 cooling fan part number.

Product Line:
ATV61

Environment:
ATV61HD30N4

Cause:
Requires a cooling fan replacement

Resolution:
VZ3V1206 is the heatsink fan kit.  The fans measure 3.62 by 3.62 inches each.  The kit contains two fans and this drive uses one fan kit per drive.  The fans are not available individually, it is only available as a kit.

Schneider Electric Česká republika

Zjistěte více
Řada:
Produkt:
Užitečné články
Zjistěte více
Řada:
Produkt: