Issue:
Needs to reset the fault over modbus on the ATS22 soft starter.
Product Line:
Altistart ATS22
Environment:
All
Cause:
Fault reset over modbus
Resolution:
The CMD register is word 752. If you set bit 3 to a 1 on the CMD word it will reset any resetable faults.
Publikováno pro:Schneider Electric Česká republika