SPM Web Application Diagrams Display the Message "The stylesheet is too complex"
Issue
Browsing the Diagram Application in Web applications displays the error message "The stylesheet is too complex"

Product
StruxureWare Power monitoring (SPM) 7.0.1

Environment
.Net Framework 4.5 and later

Cause
With changes to the .Net Framework in 4.5, if a diagram has more than 170 status objects on a single page this error message is displayed.

Resolution
SPM 7 does not officially support .Net 4.5. This issue does not occur if using .Net 4.0 or later versions of Software.

Schneider Electric Česká republika

Zjistěte více
Řada:
Užitečné články
Zjistěte více
Řada: